Johnson Controls reveals GLAS®, a beautiful thermostat for an efficient and comfortable space


GLAS tracks indoor and outdoor air quality while intuitively monitoring your schedule.

 

 

FOR IMMEDIATE RELEASE

MILWAUKEE – (Jan. 4, 2018)Johnson Controls today revealed GLAS—a simple-to-use, yet powerful smart thermostat. Designed by the same company that invented the room thermostat, GLAS leverages more than 135 years of insights in building control systems to create a thermostat with an efficient and modern perspective.

GLAS is the first smart thermostat of its kind to utilize a translucent OLED touchscreen display to control its functions. Users simply touch the screen to change the temperature, monitor indoor and outdoor air quality, track energy savings or perform other functions. Alternately, GLAS can be controlled by mobile app or by voice, thanks to Microsoft’s voice-enabled digital assistant, Cortana. When it’s not in use, the screen seamlessly blends in with a home or building’s environment.

“Developing GLAS really allowed our team to think outside of the box, understand consumers and create a customer-backed design that is both beautiful in form and also very functional,” said Don Albinger, vice president & general manager, building automation systems, Johnson Controls. “We wanted to take our experience of designing thermostats for industrial applications and enhance the features, function and user interface of the thermostat to create a more efficient and innovative way to control a space. Given that we invented the room thermostat back in the late 1800s, it’s something that Johnson Controls is naturally oriented to do.”

 

Thermostat reports indoor and outdoor air quality to help you maintain a healthy home

GLAS tracks and assesses multiple aspects of air quality to ensure that occupants are consistently comfortable, knowing that a healthy home starts with the air its residents breathe. In addition to temperature, GLAS reports humidity, total volatile organic compounds (tVOC) and equivalent carbon dioxide (eCO2) inside a home or building. When it is internet-connected, GLAS also monitors tree, grass and ragweed pollen count; ultraviolet (UV) index; and air quality index (AQI)—including carbon monoxide, sulfur dioxide, nitrogen dioxide and ozone levels. When air quality falls below moderate levels, GLAS can intelligently operate a fan or ventilation equipment. These insights arm allergy and asthma sufferers with information they need to live more comfortably.

GLAS adapts to a user’s schedule to intuitively and attentively maintain a comfortable space while it saves energy. Its automation programming is easy to understand and takes the hassle out of setting individual preferences. After a user sets preferred temperatures for Home, Away and Sleeping, GLAS’ smart logic helps save energy by detecting when a home is occupied or empty, and automatically adjusts its settings accordingly.

 

Microsoft’s Cortana and GLAS’ mobile apps allow easy control of thermostat features

With Cortana, Microsoft’s personal digital assistant, GLAS makes communicating with a user’s home simple and interactive. Users can easily adjust, refine and redefine their space with simple voice control. Cortana allows users to check and audibly receive indoor and outdoor temperatures, set increases or decreases in thermostat temperature and obtain the current weather forecast by using their voice, among other skills.

Additionally, GLAS provides an intuitive, engaging experience whether interacting with the device itself or the GLAS app on mobile, tablet or web browser. Using mobile apps for iOS and Android operating systems, users can seamlessly access GLAS controls and statistics with the same interface from the device, eliminating any learning curve.

 

GLAS leverages trusted Windows 10 IoT Core, Microsoft Azure cloud platform and power-efficient Qualcomm processor

Microsoft is a leading provider of IoT services for devices, software and cloud. GLAS utilizes the global scale and trusted Azure IoT cloud platform and Windows 10 IoT Core, leveraging the Windows platform, security and update infrastructures. Together, Windows 10 IoT Core and the Azure cloud platform provide secure, intelligent, world-class technology systems for connected buildings and homes.

GLAS is powered by the Qualcomm® Snapdragon™ 410E embedded platform that combines quad-core processing capability, Wi-Fi® and Bluetooth® connectivity in an integrated system-on-chip solution, reducing system complexity while supporting small form factors. The Snapdragon 410E is designed with high performance, energy efficiency, multimedia features and integrated connectivity that help GLAS meet the demanding requirements of its building automation and industrial control applications.

 

Temperature automation can save energy costs for users

GLAS is designed to create a consistently comfortable space and does so by leveraging Johnson Controls’ deep experience in automation and proprietary temperature control algorithms. GLAS provides around-the-clock reporting of equipment run-time as well as a related seven-day trailing report of a user’s energy savings. GLAS also provides seven-day scheduling that can be customized according to user preferences. Comfort settings include pre-start heating/cooling and fan and ventilation options based on temperature and air quality.

 

GLAS’ versatility allows for residential and commercial installations

GLAS can be installed in residential settings as well as commercial applications, such as office buildings or retail stores. Johnson Controls understands that contractors, engineers, facility managers and others involved in commercial HVAC specifications have exacting standards for their buildings, which is why it has been proud to meet or exceed those standards for over a century. As such, GLAS has been designed to adapt to a wide range of installations, including commercial buildings.

The thermostat supports most 24VAC heating and cooling systems, including most gas, electric, oil, radiant and forced air systems. It supports one and two stage conventional heating and cooling as well as heat pumps and single-speed fans, and has an auxiliary output to control humidifiers, dehumidifiers, ventilators, energy recovery ventilators or heat recovery ventilators. The low-profile, 5.6” x 5” unit and the OLED screen features an integrated touch controller and crisp resolution.

 

Product available in the first quarter of 2018

GLAS is available for pre-order in March 2018 at glas.johnsoncontrols.com and has a manufacturer’s suggested retail price of $319. For more information, visit glas.johnsoncontrols.com.

 

About Johnson Controls

Johnson Controls is a global diversified technology and multi-industrial leader serving a wide range of customers in more than 150 countries. Our 120,000 employees create intelligent buildings, efficient energy solutions, integrated infrastructure and next generation transportation systems that work seamlessly together to deliver on the promise of smart cities and communities. Our commitment to sustainability dates back to our roots in 1885, with the invention of the first electric room thermostat. We are committed to helping our customers win and creating greater value for all of our stakeholders through strategic focus on our buildings and energy growth platforms. For additional information, please visit www.johnsoncontrols.com or follow us @johnsoncontrols on Twitter.

About Johnson Controls Building Technologies & Solutions
Johnson Controls Building Technologies & Solutions is making the world safer, smarter and more sustainable – one building at a time. Our technology portfolio integrates every aspect of a building – whether security systems, energy management, fire protection or HVACR – to ensure that we exceed customer expectations at all times. We operate in more than 150 countries through our unmatched network of branches and distribution channels, helping building owners, operators, engineers and contractors enhance the full lifecycle of any facility. Our arsenal of brands includes some of the most trusted names in the industry, such as Tyco®, YORK®, Metasys®, Ruskin®, Titus®, Frick®, PENN®, Sabroe®, Simplex® and Grinnell®. For more information, visit www.johnsoncontrols.com or follow @JCI_Buildings on Twitter.

 

CONTACT: Ryan Nolan

Global Public Relations Program Manager

Building Technologies & Solutions, Johnson Controls

Work + 1 414 524 6170

Mobile + 1 414 378 9641

Ryan.P.Nolan@jci.com

 

Qualcomm and Snapdragon are trademarks of Qualcomm Incorporated, registered in the United States and other countries. Bluetooth is a registered trademark of Bluetooth SIG, Inc. Wi-Fi is a registered trademark of the Wi-Fi Alliance.

Qualcomm Snapdragon is a product of Qualcomm Technologies, Inc. and/or its subsidiaries.

# # #

Order GLAS